Other Parts Discussed in Thread: AFE4404, AFE4404EVM
I'm developing a SpO2 measurement device at wrist using AFE4404 EVM and its sensor board. Unfortunately, I can not get useful PPG signal with enough SNR. I have increased the driving current of RED and IR LED, and decreased the gain of the TIA at the same time. The duty cycle was increased to 2%, the sampling rate was 100Hz and the average number was 6. The power of the AFE4404 EVM is from a laptop which is powered with its battery, the sensor board was surrounded by black tape with LED chip exposed.
I changed the position at the wrist many times, and at only one time I got some useful PPG signal. But with the same configuration, I can not repeat the results. Only I got were DC components around 0.6V to 0.8V with tiny AC components and noise.
I want to know if the LED chips (SFH7050 and NJL5513R) within the AFE4404EVM is suitable to the wrist SpO2 application? If so, are there any parameters I can tune to realize it? Many thanks!