Part Number: AFE5809EVM
Other Parts Discussed in Thread: AFE5809, AFE5808
Dear Friends,
We are trying to connect AFE5809EVM to TSW1400EVM following the AFE5809EVM user manual guidelines.
Page 8 of slou338a document explains that we need to select AFE5809_09_14b as our device, however, I cannot find this device on our device menu of HSDC Pro software. So, instead of that I choose AFE5809 on the device menu. It seems that the firmware is downloaded and the device is connected properly. The following photo shows the LEDs after selecting ADE5809 from the device menu.
Notes:
1. We are providing the power for TSW1400EVM from the JP6 of AFE5809EVM. Our power supply provides +5v with 3A, so it should be enough for both devices. The power supplied to TSW1400EVM is +5v and ground. The power supplied to AFE5809EVM is +5v, ground, and -5v.
2. As seen in the photo, 2 out of total 8 LEDs are off. User LED 4 and 5 (D6 and D7).
3. We are not yet providing any analog signal inputs to the device.
Questions:
By using HSDC Pro software, I set the ADC output data rate to 40M and ADC input Target Freq. to 2M, then I click on capture button and I receive the following error. What does this error mean and how can I solve it?