This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300: Frequencies IQ mode is supported

Part Number: AFE4300

It appears from reviewing the AFE4300 datasheet and other documents, that IQ mode can only be run at 8, 16, 32, 64, or 128 kHz since the IQ demodulator clock divider can only be set to divide by 2, 4, 8, 16, or 32 and the IQ demodulator clock must be 4 times the frequency.  Is this correct?  I have a need to read the phase at other frequencies (such as 50, 100, and 150 kHz), is this possible?