Part Number: AFE4300
I have a problem in getting the ti AFE4300 start the ADC measurement. I started with a new board that was designed using reference design on TI. Am trying to communicate with the board through an stm32f103rbt6.
I was set up spi mode 1 and want to use body composition measurement (BCM).
I give 1mHz to afe 4300 board by arm pwm signal.
These are what has happened
1. I can not read ADC data result register.
2. the RDY pin status unchanged. it keep high status.
int main()
{
SystemInit();
UART2_Init();
DelayInit();
PWM_Init();
RESET_init();
init_spi1();
resetAFE4300();
initAFE4300();
initBCM();
//
while(1)
{
if(GPIO_ReadInputDataBit(GPIOC,PIN_DRDY) == 1){
printf("register_Name\n\r");
printf("0x%X\n\r",readRegister(ADC_DATA_RESULT));
printf("0x%X\n\r",readRegister(ADC_CONTROL_REGISTER));
printf("0x%X\n\r",readRegister(MISC1_REGISTER));
printf("0x%X\n\r",readRegister(MISC2_REGISTER));
printf("0x%X\n\r",readRegister(DEVICE_CONTROL_1));
printf("0x%X\n\r",readRegister(ISW_MATRIX));
printf("0x%X\n\r",readRegister(VSW_MATRIX));
printf("0x%X\n\r",readRegister(IQ_MODE_ENABLE));
printf("0x%X\n\r",readRegister(WEIGHT_SCALE_CONTROL));
printf("0x%X\n\r",readRegister(BCM_DAC_FREQ));
printf("0x%X\n\r",readRegister(DEVICE_CONTROL_2));
printf("0x%X\n\r",readRegister(ADC_CONTROL_REGISTER_2));
printf("0x%X\n\r",readRegister(MISC3_REGISTER));
}
else if(GPIO_ReadInputDataBit(GPIOC,PIN_DRDY) == 0){
//printf("%0x\n\r",readRegister(ADC_DATA_RESULT));
printf("low\n\r");
}
DelayMs(100);
}
}
void RESET_init(void){
GPIO_InitTypeDef GPIO_InitStructure;
//GPIO_PinRemapConfig(GPIO_Remap_SWJ_NoJTRST, ENABLE);
//GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);
/* Enable the GPIO Clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);
/* Configure the GPIO pin */
GPIO_InitStructure.GPIO_Pin = PIN_RESET;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = SPI_CS_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = PIN_DRDY;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
//
GPIO_SetBits(GPIOA, GPIO_Pin_4);
}
uint32_t RDY_read(void){
return GPIO_ReadInputDataBit(GPIOC,PIN_DRDY);
}
void RESET_HIGH(void){
//GPIOA->BSRR = PIN_RESET;
GPIO_SetBits(GPIOC,PIN_RESET);
}
void RESET_LOW(void){
//GPIOA->BRR = PIN_RESET;
GPIO_ResetBits(GPIOC,PIN_RESET);
}
void resetAFE4300(void){
RESET_LOW();
//printf("111");
DelayMs(100);
RESET_HIGH();
}
void init_spi1(void){ // for MASTER mode
GPIO_InitTypeDef GPIO_InitStructure;
SPI_InitTypeDef SPI_InitStructure;
// GPIO_StructInit (& GPIO_InitStructure);
// SPI_StructInit (& SPI_InitStructure);
/* Enable GPIOs clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
/* Enable SPI clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
/* Configure SPI SCK pin */
GPIO_InitStructure.GPIO_Pin = SPI_SCK_PIN | SPI_MOSI_PIN | SPI_MISO_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* SPI configuration -------------------------------------------------------*/
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_32; //32
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI1, &SPI_InitStructure);
/* Enable SPI */
SPI_Cmd(SPI1, ENABLE);
}
void writeRegister(unsigned char address, unsigned int data){
unsigned char firstByte = (unsigned char)(data >> 8);
unsigned char secondByte = (unsigned char)data;
GPIO_ResetBits(GPIOA, GPIO_Pin_4);
SPI_SendByte(address);
SPI_SendByte(firstByte);
SPI_SendByte(secondByte);
GPIO_SetBits(GPIOA, GPIO_Pin_4);
}
int readRegister(unsigned char address){
int spiReceive = 0;
uint8_t spiReceiveFirst = 0;
uint8_t spiReceiveSecond = 0;
address = address & 0x1F; //Last 5 bits specify address
address = address | 0x20; //First 3 bits need to be 001 for read opcode
GPIO_ResetBits(GPIOA, GPIO_Pin_4);
SPI_SendByte(address);
spiReceiveFirst = SPI_SendByte(0x00);
spiReceiveSecond = SPI_SendByte(0x00);
GPIO_SetBits(GPIOA, GPIO_Pin_4);
spiReceive = (spiReceiveFirst << 8);
spiReceive |= spiReceiveSecond;
return spiReceive;
}
void initAFE4300(void)
{
writeRegister(ADC_CONTROL_REGISTER,0x5140);
writeRegister(MISC1_REGISTER,0x0000); //
writeRegister(MISC2_REGISTER,0xFFFF); //
writeRegister(DEVICE_CONTROL_1,0x0004); //Power down both signal chains
writeRegister(ISW_MATRIX,0x0000);
writeRegister(VSW_MATRIX,0x0000);
writeRegister(IQ_MODE_ENABLE,0x0000); //
writeRegister(WEIGHT_SCALE_CONTROL,0x0000);
writeRegister(BCM_DAC_FREQ,0x0040); //
writeRegister(DEVICE_CONTROL_2,0x0000);
writeRegister(ADC_CONTROL_REGISTER_2,0x0011);
writeRegister(MISC3_REGISTER,0x00C0);
}
void initBCM(void)
{
writeRegister(ADC_CONTROL_REGISTER,0x4120); //Differential measurement mode, 32 SPS //4120//C1A0
writeRegister(DEVICE_CONTROL_1,0x0006); //Power up BCM signal chain
writeRegister(ISW_MATRIX,0x0408); //Channels IOUTP1 and IOUTN0
writeRegister(VSW_MATRIX,0x0408); //Channels VSENSEP1 and VSENSEN0
writeRegister(ADC_CONTROL_REGISTER_2,0x0063); //ADC selects output of BCM-I output
writeRegister(WEIGHT_SCALE_CONTROL,0x0000); //Gain = 1 DAC Offset = 0 0x603F
writeRegister(BCM_DAC_FREQ,0x0032);
writeRegister(MISC3_REGISTER,0x0030);
}
uint8_t SPI_SendByte(uint8_t Data)
{
while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI1, Data);
while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);
return SPI_I2S_ReceiveData(SPI1);
}
Any leads would be of great help