Other Parts Discussed in Thread: DRV8312, TMS320F28030
Hi
I want to rotate a 12V 30A BLDC motor at a speed as low as 1 RPM. Previously I have done rotation at a min of 200 rpm using the same motor with 3-hall sensors using the DRV8312 kit. We had used the usual 6 commutation state strategy for doing this.
But now since the target rpm is in a very low range, I would like to know what kind of control strategy we can use? Presently we are targeting to run the motor without any load.
For position sensing we will be using the AS5132 chip which gives absolute position feedback with a 1 degree angular resolution.
From this link www.berryjam.eu/.../
I understand the maybe SPWM can be a solution but I am not able to understand how!
Any help or guidance would be greatly appreciated!
cheers
Sanket