I am planning to use DRV8840 as peltier controller of rating 12V,3A. Is this good option to go with DRV8840?
I CHOP is 5A, with Rsense = 100 mOhm, Vref = 2.475
What extra precautions should i take if i want to design using DRV8840?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am planning to use DRV8840 as peltier controller of rating 12V,3A. Is this good option to go with DRV8840?
I CHOP is 5A, with Rsense = 100 mOhm, Vref = 2.475
What extra precautions should i take if i want to design using DRV8840?
In my application, currently I was using L6203 IC ( Full Bridge Driver with max pulse current 5A and frequency 100 kHz max ), but above ic doesn't have OCP, short ckt in-built. So I come across DRV8840 with 5a current, 100kHz max.
How much impact it will have if i chose drv8840 with 100KHz max? Do you mean, it will not work at all?
Link for L6203 which I was using in our instrument currently:

Thank you in advance.
I have GPIO limitation .. so , if I have to hardwire I0 to I4 pins,Can I do that? which is best way to do that but using current protection at the same time? ( All 0's or all 1's at I0 to I4 points )
PELTIER HUIMAO TES1-12703T125.pdf
I have attached datasheet here. Please suggest. It is customized type peltier. Thanks