Dear TI Support team,
I am evaluating DRV10983 designed using an application circuit for the ceiling fan. I configured the registers as suggested by Tuning guide and by using the Motor parameters.Speed control is done using External PWM signal from the controller. It works fine ,I could achieve the max rpm and even the speed control using PWM . I have used IPD for the position detection,enabled ISD and all other parameters using tuning guide and could achieve sufficient startup and commutation.
There is an issue that when we switch off the fan and switch on before it gets stationary ,it is not driving until it gets stationary/motor stop completely (i.e start up and commutation is not happening if it has some initial speed) . I have enabled the ISD and verified all the ISD threshold values but I couldn't solve the issue. Could you tell me is/are there any parameters other than ISD could resolve the issue?
Motor parameters for your reference
Motor resistance 1.54ohms
Motor Kt 415mv/hz
Maximum speed 385 rpm
Operating Voltage 24V
Maximum Current 1.45A
Kindly provide us the solution ASAP
Best regards,
Sathwik