Greatings! I`m running 6 Nema 17 stepper motors with 6 DRV8711 drivers. I`ve connected IRF530 MOSFETs. My pwm frequency is 4k to 12kHz. The current through the motors is set to 1.44A, 100us OFF, automix decay(I can write down all my settings if it`s necessary ). I`m recieving all driver block after 30-60 min of work instantly. All of them simultaneously. Multiple errors in all stat registers. I suppose the problem is in the power supply, but I want to be sure. Is there a way dv/dt or di/dt to cause this problems. In high power devices this is possible, but I`m not sure for such small powers. I`m using 12V computer power supply(250W).
Can you give me an advice?
Thanks!