Other Parts Discussed in Thread: DRV8305
Hi I' m Massimo,
We are using DRV 10983 for driving a 12 Vcc 10000 rpm fan motor .
With the follow configuration we are able to spinning the motor but we are to reach 6500 rpm not more , when we try to increase the speed
over 6500 rpm overcurrent block is set and the motor stopped.
At 6500 rpm the maximal misured current is 1,2 A.
Please could you help to understand where is the problem
BR
Massimo