Other Parts Discussed in Thread: DRV8711, , CSD88537ND
I evaluate DRV8711 using evaluation board BOOST-DRV8711 with +24V.
During that time, several boards broke.
Cheking the cause of failure, there is large spike noise on feedback
voltage for AISENP.
Absolute maximum rating of ISENSEx pins voltage defined from -0.7V to
+0.7V.
But my evaluation status, this voltage is over 2V and under -3V.
"please see attached pictures."
Does this spike noise cause of failure?
Does this input signal accept or not?