Other Parts Discussed in Thread: DRV8844, DRV8840
Hi,
I have noticed that the DRV8841 outputs have a phase jitter in the range of about 400ns and I believe it might be causing micro-stepping problems. I'm driving a 3 phase stepping motor and I need each phase to faithfully follow the input AIN and BIN PWM inputs. I can see that one of the bridges in the part has a 3us delay from the other and can compensate for that, but the jitter of each phase seems to be random on each phase. Please see attached video of two of the phase.
Some additional information:
1. PWM inputs look stable
2. Driver outputs jitter with and without load.
3. DRV8841 current controller is not being used. Vref = 3.3V and Sense resistor is 0.5R. Drive Current is 600mA - 1A
Thank you.