Hi Team,
Do you have any insight into how well the DRV10987 would perform on a 24V, 2A BLDC motor which needs to control its speed anywhere from 50rpm to 2000rpm? From what I understand, the Back EMF detection and control algorithm only works at higher RPMs. Is this correct? Would the motor be able to start at an initial angular velocity of 50rpm?
Regards,
Mihir