Hi,
We would like to use TIDA-00120.
Our system is :
1. 20 V solar panel
2. Battery 12V ACID battery
We would like to configure TIDA-00120 as
1. Battery current limit 20A
2. Boost voltage 14.4V
3. Floating voltage 13.6V
4. Load current limit 12A.
I look into the source code is it correct we should modifiy the Config.C to achieve the above purpose ? would you share how to modify it? thanks!
12V ACID battery