Part Number: TIDA-00961
Hi
I want to develop 3 phase CRM PFC controller via TMS320F280049 and I have some peripheral questions to ask you.
My questions are as following
1.Could the single PWM be triggered by the CMPSS comparator while peak current greater than the sinusoidal command from DAC ?
2.Could the single PWM be tripped by the CMPSS comparator while peak current less than the zero command from DAC ?
3.Could the CMPSS comparator output be inverted by setting ? The alternative current command from DAC & inductor peak current feedback be level-shifted 1,65Vdc, it means the PWM must be tripped while negative peak current less than negative current command. In other words, the output of CMPSS comparator must be inverted when AC transfer from Positive cycle to negative cycle.
Sincerely
Jack Chung from Delta Electronics, Inc. Taiwan