Other Parts Discussed in Thread: LM5000, LMG1020
Hello!
Thanks for the Gerber and BOM given by TI website,I have the chance to test the performance of the TIDA-01573 myself. It is a wonderful design that be able to solving most problems I met,but still some questions unsolved, I will be appreciate to your help.
1. what is the resisitors R5,R6,R7,R8 used for? In my test, amostly not find the difference between removing the four resistors and placing. Are the resisitors R5,R6,R7,R8 and diode D1 a loop when the GaN FET Q1 is turned off?
2. In my test, the luminescent intensity and luminescent pulse wide of LD is not stable, this will have a strong impact on our Lidar measurement accuracy. LD is OSRAM SPL_PL90_(peak current 40A). The output GATE signal wide of XLMG1020 is 20ns or 10 ns , both having the same result. Will you please give me some advice to improve it ? The Vbus is DC 35V,0.2A offered by LM5000, the Vbus is not serious affected by oscilloscope when LD drivered.The Capacitance capacity value of C2(0.01uf),C3(0.01uf),C6、C7、C8、C9(0.1uf) is the same to BOM. Does the pulse wide accuracy of driving signal to XLMG1020 have obvious implication to the luminescent intensity?
3. It seems to be difficult to buy LMG1020 in a large number now, it is a huge risk for me.
Thanks to help and best wishes!