Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642

Other Parts Discussed in Thread: IWR1642

Dear Sir/Madam,

Good day.

I appreciate for your answer about below questions.

(1) The demo CCS projects from TI Resource Explorer are not downloadable. It either stuck at the preprocessing phase or give error reports for win32 platform (but actually we have win64). Any solution?

 

(2) Is the "Tx Power" indicated in the manual the maximum power of the radar or not?

 

(3) To achieve the best velocity resolution (in short-range of a few meters), what is the maximum chirp time of IWR1642? And the max number of chirps is 512?

 

(4) If the transmitter is not omni-directional, what is the beam angle?

 

(5) Is it safe to direct IWR1642 radar to human body or brain?

 

Regards,

 

Yu