Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About TMS320C6678 SRIO

Hi, I hane a question about subject.


Using 2 lanes out of 4 lanes, connect each port with 1 x port x 2 ports I want to independently connect with endpoint (FPGA) on a 1: 1 basis. In this case, Is it possible to operate the 1x port of C6678 independently as a host?

  • onda様、

    レインの速度を同じにする必要は有りますが(SPRUGW1B, p.2-102.3.1)、
    x2 + x2 での互いに独立した転送(Mode3)は可能です(SPRUGW1B, p.2-14
    Table2-4)。

    ・Serial RapidIO (SRIO) for KeyStone Devices User's Guide(SPRUGW1B)
    www.ti.com/.../sprugw1


    E2Eには、受けられない事象が報告されていますが、IDのマッチングが取れて
    いない事が原因の様で、この点にご注意下さい。

    なお、下記のページには、初心者向けの解説記事が置かれていますの、ご参照
    下さい。

    ・SRIO Help for Beginners (C6678 and SRIO switch)
    e2e.ti.com/.../752157

    また、幾つかの参考になりそうな、トラブルシューティング記事も、ご紹介
    させて頂きます。

    ・Send SRIO data to DSP using FPGA
    e2e.ti.com/.../554366

    ・SRIO Help for Beginners (C6678 and SRIO switch)
    e2e.ti.com/.../752157

    ・CC678 SRIO problem
    e2e.ti.com/.../200057

    ・CC678 SRIO problem
    e2e.ti.com/.../200057

    以上、宜しくお願い致します。