Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About C6678 SRIO

Hi, I have questions.

Can the following registers set the host or register?

SP_GEN_CTL Bit31  HOST


And, Is it possible to set different host and slave for each port?

  • onda様、

    ・Serial RapidIO (SRIO) for KeyStone Devices User's Guide
    www.ti.com/.../sprugw1
    p35. Figure 2-1 Peripheral Module
    p.212 3.14.20 SP_GEN_CTL

    最初に、上記のUGをご参照下さい。

    HOSTの説明はp.212に記載されていますが、主体的に通信を制御する
    場合は、bit-30(MASTER_ENABLE)を使用します。

    また、p35. Figure 2-1 Peripheral Module に描かれている様に、
    portはSERDESを含む、最下層にあって、実際の通信を司るだけです。

    ですから、制御は上位層で行われますので、各Portは異なるDestination
    に対しても、等価に利用できます。