Hello Everyone,
I'm trying to implement an EVE app that merges two 16bit values into one 32bit value. The goal is to overwrite the values from the input buffer with the new calculated ones, so that I work on only one combined in/out buffer instead of two seperate buffers. Is this possible on VCOP or does a VCOP kernel always contain a designated input and output buffer (IbufL and IbufH)?
If possible, can I "merge" IbufL and IbufH together to one buffer, so that I process 32kB instead of 16kB of data without relaoding the buffer (via EDMA)?
Regards,
Tobias