Tool/software: Code Composer Studio
Hello Team,
I am working on TDA2x module and i have to copy external file data onto cache so that it can execute faster on DSP core.
But while building project i am getting error.
I modified .cmd file as per document mentioned in "(page No. 34 )" initially i got result like "CACHE_CE00" and CACHE_256KCACHE not defined for function CACHE_enableCaching and CACHE_setL2Size,so later on i hard coded value of CACHE_CE00 as 128(0x80 : MAR128), and CACHE_256KCACHE as 0x7d00(Size : 32Kbytes) and after compilation i got result as below :
"error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "test_sobel_kernel_dsp.out" not built"
I also tried by configuring L1D and L1P but got same result.
I have included below files in .c file :
#include <ti/csl/cslr_cache.h>
#include <ti/csl/csl.h>
#include <ti/csl/soc/tda2xx/c66x/soc.h>
and in properties added path of directory of pdk/packages.
Are above added files are correct or i need to add some more files in .c ?
I am using pdk version "pdk_01_08_00_16",
I am testing on Ubuntu system 14.4,CCS7.3,TDA2x,vision sdk 3.1
Also i checked with different lnk_dsp.cmd files but got same result.
Please help me or give some pointer so i can go ahead ..........!!
Regards,
Pritam