Tool/software: TI-RTOS
Hello, I want to run Demo on VisionSDK_UserGuide_TDA2xx.pdf using HDMI input.
SDK version is 02.12.02 and CCS is 7.
I tried to set the EDID for HDMI Capture. (following Chapter 2.3.3. EDID Programming for HDMI Capture on 02.12.02 SDK UserGuide)
First of all, Change pin 1 and 2 of SW8000 (SW1 at visionSDK Guide) to ON (pin 3, 4 is OFF)
And I made new target configuration and set the bypass option except for "cortex_a15_0" at target configuration setting using CCS .
And launch the configuration file. and then load binary file named 'edid_programming_1080p_60.xa15fg' using CCS.
After running,
"I2c Probe failed!!..Please check SW1 settings"
messages are infinitely printed on hyperterminal.
================================================================================
When I run the Demo "Lane Detection" which Usecase No. "b" after changing "HDMI Capture 1080p60" mode, below error message is printed on console of CCS.
i2cMdSubmitChan: i2c1 transfer to slave address 0x4c failed
Assertion @ Line: 175 in C:/VISION_SDK_02_12_02_00/vision_sdk/examples/tda2xx/src/devices/hdmi_recvr.c: retVal == 0 : failed !!!
[Cortex_M4_IPU1_C1] Service Status: DHCPC : Enabled : Fault : 002
================================================================================
I just want to run the Demo to know how to use this board.
But it is not easy to me.
How can I solve this problem??
Thank you in advance.