Tool/software: Code Composer Studio
When I compile a EVE project which include k files in ccs 7.4, The linker show the error ?
How can I solve it?
undefined first referenced
symbol in file
--------- ----------------
vcop_blockAverage2x2_uchar_cn ./main.obj
vcop_gauss5x5PyramidKernel_8_horiz_c ./main.obj
vcop_gauss5x5PyramidKernel_8_vert_c ./main.obj
error #10234-D: unresolved symbols remain
warning #10063-D: entry-point symbol other than "_c_int00" specified: "_reset_handler"
error #10010: errors encountered during linking; "imagePyd.out" not built
>> Compilation failure
makefile:153: recipe for target 'imagePyd.out' failed
gmake[1]: *** [imagePyd.out] Error 1
makefile:149: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****