Tool/software: Linux
Hello,
I am running PROCESSOR_SDK_VISION_03_01_00_00 Linux running on the tda2evm5777 and I need to set all linux processes to a single A15 (A15_0), including and in particular, the ethernet driver. This is so I can expect less interrupts from Linux when running my own applications on the second A15 (A15_1)
When I run the taskset command to set the cpu affinity for all of the processes in linux to go on A15_0, some processes do not change cpu affinity.
I have tried isolcpus, but not all processes get changed to be on A15_0.
How can I force all processes to be on A15_0, including the ethernet driver, so I can run my own program,on A15_1 and have those be the only things running in linux on that core?
How can I set the ethernet driver to run only on A15_0?