Part Number: TPS82130
Hello, I'm having an issue with my TPS82130. I believe I've accidentally entered the Low Dropout Operation mode as described in the datasheet. I'm guessing it's an issue with part values in the feedback network. This part has worked fine for me in the past in this circuitry.
Using a multimeter I don't ohm a short between the input and outputs of this switcher... but I do read almost the same voltage when enabled. Which is leading me to believe that the high side fet is stuck on. Could you please provide more information on this mode. It's unclear if this is something automatic or something that i've accidentally triggered. Thanks.