Tool/software: Linux
Dear,
1. ISS capture -> ISSM2mIsp -> Alg_IssAewb
ISSM2mIsp -> Select_Capture -> Merge_Simcop->Dup_Simcop->Display_Video
Select_Capture->ISSM2mSimcop->Merge_Simcop
Above use case runs well.
But, if I add Sync between Dup_Simcop and Dispaly_Video the display screen is black.
In Sync paramter function,
I set only two parameters which are
static Void setSyncLinkParams(
SyncLink_CreateParams *pPrm,
UInt32 numCh,
UInt32 syncPeriod)
{
pPrm->syncDelta = SYNC_DELTA_IN_MSEC; //16
pPrm->syncThreshold = SYNC_DROP_THRESHOLD_IN_MSEC; //33
}
What is problem?
Thanks,
Best regards,
Heechang