Looking for a sample project to simply toggle the J16 (MAVRK CONNECTOR) GPIO1_D0 PIN using SYS/BIOS
I've seen the SYS/BIOS videos but the example don't seem to cover the AM335x (Sitara) processor. I've tried the examples from the Starterware (../ti\AM335X_StarterWare_02_00_01_01\platform\evmAM335x) . Most of the projects seem to use Beaglbone or Linux. I have also tried the PINMUX programs to set up the pins with no luck.
Could someone provide sample code or link?
My Environment:
Windows 7 with CCS6.x; SYS/BIOS
Using AM3358 EVM (Note the actual processor is AM3359) with the TI XDS2xx USB Debug Probe
Thanks