I use C28335 in my products. and xintf zone0 connect to fpga(lattice xp2-8), zone6 connect to cpld,zone7 connect to a sram.
the xintf config as follow:
EALLOW;
XintfRegs.XINTCNF2.bit.XTIMCLK = 1;
// No write buffering
XintfRegs.XINTCNF2.bit.WRBUFF = 0;
// XCLKOUT is enabled
XintfRegs.XINTCNF2.bit.CLKOFF = 0;
// XCLKOUT = XTIMCLK/2
XintfRegs.XINTCNF2.bit.CLKMODE = 0;
// Zone 0------------------------------------
// When using ready, ACTIVE must be 1 or greater
// Lead must always be 1 or greater
// Zone write timing
XintfRegs.XTIMING0.bit.XWRLEAD = 3;
XintfRegs.XTIMING0.bit.XWRACTIVE = 7;
XintfRegs.XTIMING0.bit.XWRTRAIL = 3;
// Zone read timing
XintfRegs.XTIMING0.bit.XRDLEAD = 3;
XintfRegs.XTIMING0.bit.XRDACTIVE = 7;
XintfRegs.XTIMING0.bit.XRDTRAIL = 3;
// double all Zone read/write lead/active/trail timing
XintfRegs.XTIMING0.bit.X2TIMING = 0;
// Zone will sample XREADY signal
XintfRegs.XTIMING0.bit.USEREADY = 0;//;
XintfRegs.XTIMING0.bit.READYMODE = 0; // sample asynchronous
// Size must be either:
// 0,1 = x32 or
// 1,1 = x16 other values are reserved
XintfRegs.XTIMING0.bit.XSIZE = 1;
// Zone 6------------------------------------
// When using ready, ACTIVE must be 1 or greater
// Lead must always be 1 or greater
// Zone write timing
XintfRegs.XTIMING6.bit.XWRLEAD = 3;
XintfRegs.XTIMING6.bit.XWRACTIVE = 7;
XintfRegs.XTIMING6.bit.XWRTRAIL = 3;
// Zone read timing
XintfRegs.XTIMING6.bit.XRDLEAD = 3;
XintfRegs.XTIMING6.bit.XRDACTIVE = 7;
XintfRegs.XTIMING6.bit.XRDTRAIL = 3;
// double all Zone read/write lead/active/trail timing
XintfRegs.XTIMING6.bit.X2TIMING = 0;//
// Zone will sample XREADY signal
XintfRegs.XTIMING6.bit.USEREADY = 0; //;The XREADY signal is ignored when accesses are made to the zone.
XintfRegs.XTIMING6.bit.READYMODE = 0; // sample asynchronous
// Size must be either:
// 0,1 = x32 or
// 1,1 = x16 other values are reserved
XintfRegs.XTIMING6.bit.XSIZE = 1;
// Bank switching
// Assume Zone 7 is slow, so add additional BCYC cycles
// when ever switching from Zone 7 to another Zone.
// This will help avoid bus contention.
XintfRegs.XBANK.bit.BANK = 6;
XintfRegs.XBANK.bit.BCYC = 7;
EDIS;
The problem is :
when my project runs as debug mode(use ccs4.2 to build by debug configration),everything is ok. but when I change to release configration(or the optimization change to 2), The reg's data which in zone6 maybe error.It looks like I write the regs,but I only read the regs.
please give me some abvice,thank you very much!