Other Parts Discussed in Thread: AM3358
Tool/software: Linux
I am using AM335x Start-Kit, TMDSSK3358 and I am trying to use PROCESSOR-SDK-AM335X but every time SD boot failed with following message
U-Boot SPL 2016.05 (Feb 20 2017 - 16:27:15)
Trying to boot from MMC1
** First descriptor is NOT a primary desc on 0:1 **
** Partition 1 not valid on device 0 **
spl_register_fat_device: fat register err - -1
** Partition 1 not valid on device 0 **
spl_register_fat_device: fat register err - -1
spl_load_image_fat: error reading image u-boot.img, err - -1
spl: no partition table found
spl: no partition table found
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
so I did test about MLO, changed Android MLO to Linux MLO but it was same
but SD Boot on the Android was so different if I used Linux MLO or Android MLO on the Android , SD boot was working properly
so I think this problem is partition problem or other problem.
I used TI-Image and Win32DiskImager Program
Thanks for reading my message