Other Parts Discussed in Thread: TMDXIDK5718, TMDSEVM572X, BEAGLEBOARD-X15, AM5728, PMP
Tool/software: Linux
Hi Team,
We have procured TMDXIDK5718 and TMDSEVM572X development boards from TI.
I have downloaded ti-processor-sdk-linux-am57xx-evm-03.03.00.04-Linux-x86-Install.bin and able to run it successfully on Ubuntu 14.04. I have used the setup.sh for installing necessary packages, thanks for making things easy.
My interest is to use same kernel source for two different CPU variants that is AM571x & AM572x.
Following are my questions:
1) How do I choose the LOADADDR for kernel compilation,
from the u-boot/include/configs/am57xx.h I did not get details about LOADADDR, please help.
2) I have chosen tisdk_am57xx-evm_defconfig for building kernel, from the .config I see it is for SMP kernel that is AM572x, is this the right one?
3) How about kernel config for AM571x based EVM ?? Its just to disable SMP or through u-boot parameters
4) am57xx_evm_defconfig is the right config for building u-boot.
5) I read kernel image files should be part of rfs instead of boot FAT partition, correct me if I am wrong.
Please help me with your inputs.