Hello,
I have a Beaglebone black and I've flashed the SDK image on an SD card using this method http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Creating_a_SD_Card_with_Windows
I am able to boot into the Arago Project screen and able to log in as root. When I attach a monitor to the HDMI port, a please wait screen is persistent and does not change. I've tried starting and stopping the matrix-gui-browser-2.0 as well as restarting the weston service. I've also tried attaching a Beaglebone black compatible LCD cape (works on debian image) which also just lights up all white but does not show the GUI or the "please wait" screen.
Please advise what to try next.
Thanks
Date: 2017-03-29 UTC
[20:53:59.333] weston 1.9.0
http://wayland.freedesktop.org
Bug reports to: https://bugs.freedesktop.org/enter_bug.cgi?produc
Build: 1.8.93-2-gb05cdb8 configure.ac: bump to version 1.9.0 for
[20:53:59.333] OS: Linux, 4.4.41-gf9f6f0db2d, #1 PREEMPT Wed Mar 29 17:37:15 EDT
[20:53:59.336] Using config file '/etc//weston.ini'
[20:53:59.346] Loading module '/usr/lib/weston/drm-backend.
[20:53:59.454] Output repaint window is 7 ms maximum.
[20:53:59.454] initializing drm backend
[20:53:59.466] using /dev/dri/card0
[20:53:59.492] Loading module '/usr/lib/weston/gl-renderer.so'
failed to load module: /usr/lib/gbm/gbm_dri.so: cannot open shared object file:
failed to load module: /usr/lib/gbm/gbm_gallium_drm.so: cannot open shared objec
loaded module : gbm_pvr.so
found valid GBM backend : gbm_pvr.so
[20:53:59.625] warning: either no EGL_EXT_platform_base support or specific plat
[20:53:59.699] warning: EGL_EXT_buffer_age not supported. Performance could be a
[20:53:59.699] Retrieving EGL client extension string failed.
[20:53:59.701] warning: no input devices on entering Weston. Possible causes:
- no permissions to read /dev/input/event*
- seats misconfigured (Weston backend option 'seat', udev device propert
[20:53:59.701] failed to create input devices
trying to open device 'i915'...failed
trying to open device 'radeon'...failed
trying to open device 'nouveau'...failed
trying to open device 'vmwgfx'...failed
trying to open device 'omapdrm'...failed
trying to open device 'exynos'...failed
trying to open device 'tilcdc'...done
Encoders:
id crtc type possible crtcs possible clones
25 24 TMDS 0x00000001 0x00000000
Connectors:
id encoder status name size (mm) modes encoders
26 25 connected HDMI-A-1 480x270 18 25
modes:
name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
1280x1024 60 1280 1328 1440 1688 1024 1025 1028 1066 flags: phsync, pvsync; tr
1440x900 60 1440 1488 1520 1600 900 903 909 926 flags: phsync, nvsync; type: r
1280x800 60 1280 1328 1360 1440 800 803 809 823 flags: phsync, nvsync; type: r
1152x864 75 1152 1216 1344 1600 864 865 868 900 flags: phsync, pvsync; type: r
1280x720 60 1280 1390 1430 1650 720 725 730 750 flags: phsync, pvsync; type: r
1280x720 60 1280 1390 1430 1650 720 725 730 750 flags: phsync, pvsync; type: r
1280x720 50 1280 1720 1760 1980 720 725 730 750 flags: phsync, pvsync; type: r
1024x768 75 1024 1040 1136 1312 768 769 772 800 flags: phsync, pvsync; type: r
1024x768 60 1024 1048 1184 1344 768 771 777 806 flags: nhsync, nvsync; type: r
800x600 75 800 816 896 1056 600 601 604 625 flags: phsync, pvsync; type: drivr
800x600 60 800 840 968 1056 600 601 605 628 flags: phsync, pvsync; type: drivr
720x576 50 720 732 796 864 576 581 586 625 flags: nhsync, nvsync; type: driver
720x480 60 720 736 798 858 480 489 495 525 flags: nhsync, nvsync; type: driver
720x480 60 720 736 798 858 480 489 495 525 flags: nhsync, nvsync; type: driver
640x480 75 640 656 720 840 480 481 484 500 flags: nhsync, nvsync; type: driver
640x480 60 640 656 752 800 480 490 492 525 flags: nhsync, nvsync; type: driver
640x480 60 640 656 752 800 480 490 492 525 flags: nhsync, nvsync; type: driver
720x400 70 720 738 846 900 400 412 414 449 flags: nhsync, pvsync; type: driver
props:
1 EDID:
flags: immutable blob
blobs:
value:
00ffffffffffff001e6db85a01010101
0118010380301b78ea3135a5554ea126
0c5054a54b00714f81809500b300a9c0
810081c09040023a801871382d40582c
4500e00e1100001e000000fd00384b1e
530f000a202020202020000000fc004c
47204950532046554c4c4844000000ff
000a2020202020202020202020200164
020315b14a900403011412051f101365
030c001000023a801871382d40582c45
00e00e1100001e011d8018711c162058
2c2500e00e1100009e011d007251d01e
206e285500e00e1100001e8c0ad08a20
e02d10103e9600e00e11000018000000
00000000000000000000000000000000
000000000000000000000000000000b4
2 DPMS:
flags: enum
enums: On=0 Standby=1 Suspend=2 Off=3
value: 0
CRTCs:
id fb pos size
24 29 (0,0) (1280x1024)
1280x1024 60 1280 1328 1440 1688 1024 1025 1028 1066 flags: phsync, pvsync; tr
props:
Planes:
id crtc fb CRTC x,y x,y gamma size possible crtcs
23 24 29 0,0 0,0 0 0x00000001
formats: RG16 BG24 XB24
props:
5 type:
flags: immutable enum
enums: Overlay=0 Primary=1 Cursor=2
value: 1
Frame buffers:
id size pitch