Hi all,
I'm trying QSPI boot with reference to Booting Via QSPI on the link below.
processors.wiki.ti.com/.../AM437x
But the device will not boot QSPI.
I prepared Flash Device and output the following message.
--------------------------------------------
StarterWare QSPI Flash Writer!!
BOARDInit status [0x0]
SoC : [AM43XX]
Core : [A9]
Board Detected : [IDKEVM]
Base Board Revision : [UNKNOWN]
Daughter Card Revision: [UNKNOWN]
Copying boot to QSPI Flash
Copying app to QSPI Flash
Changing read to quad mode
Read mode has been changed to Quad mode
SUCCESS!!!
Flashing completed
--------------------------------------------
But "Booting the targe" of web link does not work.
I was able to put the following three files in the SD card and copy it to QSPI.
(1) C:\ti\pdk_am437x_1_0_6\packages\ti\starterware\tools\qspi\config
(2) C:\ti\pdk_am437x_1_0_6\packages\ti\starterware\binary\gpio_app_led_blink\bin\am43xx-evm\gcc\gpio_app_led_blink_a9host_debug_ti.bin
(I Renamed the following file to "app".)
(3) C:\ti\pdk_am437x_1_0_6\packages\ti\starterware\binary\bootloader\bin\am43xx-evm\gcc\bootloader_boot_qspi_a9host_debug.bin
(I Renamed the following file to "boot".)
What else should I do?
Best regards,
Sasaki