This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5401: Slope Comp and Current Limit Details

Part Number: TPS5401

Hello,

For the TPS5401, can we share the internal slope compensation values so the customer can design the rest of the circuit in accordance with those values?

Also, this application will require just under 600mA peak switch current, which is close to the min current limit spec. We want to avoid entering current limit mode unintentionally. The .6A min current limit spec is at 25C, will the spec increase or decrease as temperature increases?

Thanks!

Ryan B.