Hello, Tom here, brand new user of AM3359 ICE dev kit.
I've followed the instructions in the "AM3359 Industrial communications engine for Industrial Automation Quick Start Guide" (SPRW231A) to the final bullet point on page 2: "Now the user can control digital out LEDs using twinCAT. Select Box n (TIESC-001)..." but when I change the values in the write command between 0 and 255 (0xff) the "digital output" LEDs on the ICE board don't change state.
- I think the etherCAT bus has reached the OP state because "ethernet LED" D1 led is ON solid green, D2 OFF. Speed LED D4 ON solid amber.
- the state of the "digital output" leds when the board powers up is D7,D8,D10,D14 ON all others OFF. And this doesn't change, regardless of what I write to the 32 bit RPDO. Example: request for all LEDs on (255)
Any ideas as to what might be wrong? Is it possible the board wasn't flashed with demo software? Any suggestion as to what I might try next?