Part Number: BEAGLEBK
Tool/software: Code Composer Studio
Hello,
I'm trying to run the UartEcho starterware example on CCS6 running on Ubuntu 16.04 with a BeagleBone Black. I'm connected to the Beaglebone over an XDS200 JTAG.
Here's what I've done so far:
1. I used File -> Import -> CCS Projects
2. imported drivers, platform, system, utils, and uartEcho.
3. Set each project Properties -> General -> Device to BeagleBone_Black [Cortex A]
4. Cleaned and Build all projects
5. With uartEcho as the active project, select Run -> Debug
6. The CCS Debug perspective opens and I use F6 to step through each line of code.
At MMUConfigAndEnable() -> CP15TlbInvalidate() the processor jumps to 0x20080 - Undefined exception default handler Dead Loop
I've tried this on two different BeagleBones and get the same results.
Is there additional project set up that I missed? Shouldn't this work?