Tool/software: Linux
Dear Friends
I have a problem during execution of bitbake command in
I want to install qtserial port on qt5 in ti sdk so i followed the instruction in below Thread
Linux/AM5728: Qt serial port
$ sudo apt-get install git build-essential python diffstat texinfo gawk chrpath dos2unix wget unzip socat doxygen libc6:i386 libncurses5:i386 libstdc++6:i386 libz1:i386
$ sudo dpkg-reconfigure dash
# Select "No" when prompted.
$ wget releases.linaro.org/.../gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf.tar.xz
$ tar -Jxvf gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf.tar.xz -C $HOME
$ git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
$ cd tisdk
$ ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-04.02.00.09-config.txt
$ cd build
$ . conf/setenv
$ export PATH=$HOME/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:$PATH
$ MACHINE=am57xx-evm bitbake qtserialport
Now I got an error during last command "MACHINE=am437x-evm bitbake qtserialport"
Here is my message log
WARNING: linux-libc-headers-4.9-r0.arago2 do_fetch: Failed to fetch URL git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=ti-lsk-linux-4.9.y, attempting MIRRORS if available ERROR: linux-libc-headers-4.9-r0.arago2 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-2uZ0tDpHHk"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/vivek/tisdk/sources/oe-core/scripts:/home/vivek/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/arm-linux-gnueabi:/home/vivek/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/am57xx-evm/usr/bin/crossscripts:/home/vivek/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/vivek/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/vivek/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/vivek/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/home/vivek/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/vivek/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/vivek/tisdk/sources/meta-ros/scripts:/home/vivek/tisdk/sources/meta-browser/scripts:/home/vivek/tisdk/sources/oe-core/scripts:/home/vivek/tisdk/sources/bitbake/bin:/home/vivek/bin:/home/vivek/.local/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/vivek"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git /home/vivek/tisdk/downloads/git2/git.ti.com.ti-linux-kernel.ti-linux-kernel.git --progress failed with exit code 128, output: Cloning into bare repository '/home/vivek/tisdk/downloads/git2/git.ti.com.ti-linux-kernel.ti-linux-kernel.git'... fatal: unable to connect to git.ti.com: git.ti.com[0: 198.47.28.208]: errno=Connection refused ERROR: linux-libc-headers-4.9-r0.arago2 do_fetch: Fetcher failure for URL: 'git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git;protocol=git;branch=ti-lsk-linux-4.9.y'. Unable to fetch URL from any source. ERROR: linux-libc-headers-4.9-r0.arago2 do_fetch: Function failed: base_do_fetch ERROR: Logfile of failure stored in: /home/vivek/tisdk/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/linux-libc-headers/4.9-r0.arago2/temp/log.do_fetch.12526 ERROR: Task (/home/vivek/tisdk/sources/meta-arago/meta-arago-distro/recipes-kernel/linux-libc-headers/linux-libc-headers_4.9.bb:do_fetch) failed with exit code '1' NOTE: Tasks Summary: Attempted 327 tasks of which 325 didn't need to be rerun and 1 failed. Summary: 1 task failed: /home/vivek/tisdk/sources/meta-arago/meta-arago-distro/recipes-kernel/linux-libc-headers/linux-libc-headers_4.9.bb:do_fetch Summary: There were 2 WARNING messages shown. Summary: There were 3 ERROR messages shown, returning a non-zero exit code.
I cant say its a network issue because i can access my network without issue after run bitbake command in terminal
help me out to fix this problem
Best Regards
vivek yuvan