Other Parts Discussed in Thread: AM3352
Hello,
Regarding to LRCK,BCK on TLV320DAC3100, my customer has some question.
They use linux driver for TLV320AIC31XX.(Used DAC block.) and use AM3352 as MCU.
www.ti.com/.../TLV320AIC31XXSW-LINUX
TLV320DAC3100 is master and MCASP0(FSX ACLKX)in AM3352 is an input port.
(Question)
(1)When audio signal isn’t input to DAC from AM3352, PLL,DAC,HP DRIVE and Class-D AMP block in DAC3100 are power-down.
(They think this seems specification of linux driver.)
At that time, LRCK,BCK line between DAC3100 and AM3352 aren’t low level and this level is DC 0.8V.
Is there any problem on DAC3100 at level(DC 0.8V)? Or is it specification? (No pronlem)
When DAC3100 is power-down, are LRCK and BCK port in DAC3100 an input ?
(If so, the LRCK and BCK port of both DAC3100 and AM3352 are an input.)
(2)They want LRCK and BCK port are an output anytime in DAC3100.
Is it possible to modify to output anytime in linux driver by them?
(3) When PLL and DAC are on, HP DRIVER and Class-D DRIVER make power-down.
In this case, is there any problem on DAC3100?
Regards,
Tao_2199