Is there a reference document that explains clocking for these TLV320 DSPs?
For example, if my desired sample frequency is 48KHz, and I choose to use my own clock. I assume the MCLK is best at some integer multiplier of the sample frequency. ADC_CLKIN and DAC_CLKIN will be linked to the MCLK. In what situations would these be different frequencies? After multipliers and dividers, when all the dust settles, is the DAC_FS supposed to be at 48KHz? Is the ADC_FS always the same? What is the desired frequencies of the modulator clocks in relation to the other clocks and why? What are the miniDSP_A and mini_DSP_D clock values in relation to ADC_CLKIN or DAC_CLKIN? What is the role of DOSR and AOSR values?
Is there an application or spreadsheet that calculate these values? I see the formulas within my TLV320AIC3268 Users Guide (SLAS953A, section 8.3.4, pp 65-67) but they don't explain the end-goal of the frequency settings.
Thank you.
Phil