Hi
I need to cascade 2x PCM1840 TDM into a single TDM 8ch Buss to have 8 ADC channels to the DSP
Is the PCM1840capable of this. The datasheet is unclear. as it talks about 4ch and the ability to have 8 Digital Mics,
Thanks
Brett
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I need to cascade 2x PCM1840 TDM into a single TDM 8ch Buss to have 8 ADC channels to the DSP
Is the PCM1840capable of this. The datasheet is unclear. as it talks about 4ch and the ability to have 8 Digital Mics,
Thanks
Brett
Hi Brett,
The PCM1840 unfortunately does not provide a direct way to offset the data in the TDM stream to allow multiple PCM1840s to share the same TDM bus. In order to do this though you could use a 50% duty cycle FSYNC and invert the clock sent to one of the devices so that one outputs data on the rising edge of FSYNC and the other on the falling edge.
Best,
Zak
Hey Brett,
No data mux would be needed, but that could be another option. The PCM1840 will set the DOUT to HiZ for the BCLK cycles/slots it doesn't use and can support high enough BCLK that this shouldn't be an issue. The device fully supports TDM, it just doesn't have a way to daisy chain data lines.
Best,
Zak