This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5805M: There is no sound when playing music in TDM mode , How to configure TDM mode

Part Number: TAS5805M
Other Parts Discussed in Thread: TAS5805

Hi Ti ,

I configured TDM mode according to this document TAS58xxM TDM Configurations(16-ch, 32-bit),

Now just use a chip

reg config : 0x33 = 0x17 , 0x34 = 0x00

but now there is no sound when playing music.

Please check this issue . Thanks

Regdump:

kona:/ # i2cdump -f -y 0 0x2c                                                  
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
00: 00 00 00 03 00 00 00 00 00 00 00 00 00 00 00 00    ...?............
10: 01 00 00 00 01 00 00 00 00 00 00 00 00 00 00 00    ?...?...........
20: 01 07 09 01 00 40 02 00 00 00 00 00 00 00 00 00    ????.@?.........
30: 00 00 00 17 00 11 00 19 00 08 f9 04 00 20 80 00    ...?.?.?.???. ?.
40: 01 00 00 00 00 00 01 00 00 00 00 00 30 30 33 30    ?.....?.....0030
50: 07 00 00 00 00 00 00 00 00 00 00 00 00 f8 00 00    ?............?..
60: 00 00 00 00 00 00 00 00 03 00 00 00 00 50 11 24    ........?....P?$
70: 00 04 00 00 00 38 00 00 00 00 09 03 00 00 2a 00    .?...8....??..*.
80: 00 00 00 03 00 00 00 00 00 00 00 00 00 00 00 00    ...?............
90: 01 00 00 00 01 00 00 00 00 00 00 00 00 00 00 00    ?...?...........
a0: 01 07 09 01 00 40 02 00 00 00 00 00 00 00 00 00    ????.@?.........
b0: 00 00 00 17 00 11 00 19 00 08 f9 04 00 20 80 00    ...?.?.?.???. ?.
c0: 01 00 00 00 00 00 01 00 00 00 00 00 30 30 33 30    ?.....?.....0030
d0: 07 00 00 00 00 00 00 00 00 00 00 00 00 f8 00 00    ?............?..
e0: 00 00 00 00 00 00 00 00 03 03 00 00 00 50 11 24    ........??...P?$
f0: 00 04 00 00 00 38 00 00 00 00 09 03 00 00 2a 00    .?...8....??..*.