This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4890: LM4890 and LM4889.

Guru 10765 points
Part Number: LM4890
Other Parts Discussed in Thread: LM4889

Hi team,

 I was looking at the datasheets for the LM4890 and the LM4889 and I can’t see what the difference is between the two parts. 
Could you tell me about the differences?

Sincerely.
Kengo.

  • Hello, 

    These two parts are very similar but there are a couple slight differences. They don't both offer all the same packages. The LM4890 offers 9-bump package options that the LDM4889 does not. Additionally, there is some slight change in the device max ratings between the two. 

    Best Regards, 

    Justin Beigel