I have a TAS2563 stereo (dual mono) EVM powered by a lab supply 5V/6.4A to VBAT. I have been able to characterize the speakers. Works well with a single channel. The issue when I try to run a demo using two channels.
The setup is complete in PPC3, and music is passing through. When the volume form the PC is increased, the EVM will shutdown and the TI "soundcard" looses connection, the PPC3 does not identify the board. A power cycle and rebooting of the EVM resets the system to work again.
There is no indication of what is triggering the shutdown, is it in protection mode?
The system when on idle and ready to play has a quiescent current of 230~270mA
When the system shuts down, the quiescent current drops to ~150mA, there is no connection to the PC.
With the characterization board plugged or unplugged the behavior is the same, just different quiescent currents...
When I measure the current into the EVM using a 100mOhm shunt resistor, I see a peaks of about 4A prior to shutdown.
Questions:
(1) Should I expect the EVM to drive two 4ohm micro-speakers at max power (2x3W)??
(2) What is the protection mode that is triggered? how to debug?