This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5825PEVM-AMPS097: No available EVM Apps are shown in PPC3

Part Number: DRV5825PEVM-AMPS097
Other Parts Discussed in Thread: TPA3255, TAS5825P, TAS5825PEVM

I have installed and launched the PPC3 for the first time but do not see any available EVM apps.

Is there some other program that needs to be installed for the specific EVM?  I tried the refresh button but nothing shows up.

The DRV5825PEVM has the USB plugged in but it does not show up in the device manager.

This PP3 was downloaded upon request when I used TPA3255.

Do I have to request and download the same PP3 when I using DRV5825PEVM?

Best Regards.