Other Parts Discussed in Thread: TPA3255
Would using a filter inductor that has a saturation current lower than the TPA3255 current limit (R_OCADJ=30.1kOhm, I_OC=13A), such as UA8013-AL (Isat_10% = 12A, Isat_30%=13.2A), cause the inductors to begin to saturate, and consequently pass more switching ripple to output than would be expected if an inductor with a much higher saturation current was used?