Hi team,
My customer is asking about why the voltage rating on these caps needs to be 16V. Would you please provide your comments. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Andy
Our capacitor supplier suggest us to choose the rated voltage no less than twice the maximum voltage in our circuit. Besides, the rated voltage of 16V is more commonly used. It's not a strict restriction, our customer can ask their capacitor supplier for more suggestions.
Hi Andy
The voltage is where the capacitor placed. For example at the pin of GVDD, the voltage should be 5V with a very little ripple on it. So the rated voltage of capacitor on this pin should be larger than 10V. At the other place, the rated voltage should be also re-calculated in this way.