Other Parts Discussed in Thread: PCM1862, PCM1860, OPA1692
Dear support team,
I confirmed that and thought that the bias voltage was around 1.5 ~ 1.45V.
Seems to be sufficient for full-scale input 2Vrms.
The supply voltage of my system is 3.3VThe amplifier in the previous block is also 3.3V.That means that the amplifier output is up to 3.3V.
When a 3.3V signal enters the PCM1820, it first exceeds the specification of negative voltage limitation.
I suspect that the bias is not half the power supply. Since there is a 3.3V input under the worst conditions in the system, I would like to avoid breaking the PCM1820 low voltage limitation by halving the bias of the power supply.
Is there a way to do that?
Best regards,
Yukio Oyama