Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Hi,
I'm new in the forum. I have a question regarding the example of USB_DevAudio_lcdkOMAPL138_c674x. The example as it is already have some 'pop noises' when executed. These noises happen almost periodically (around each one second, but not exactly) when reproducing any sounds or music from the USB Audio input. This doesn't happen if there is just silence reproducing. Could it be some configuration or memory issue? It doesn't happen the other way (I implemented the mic in as an input to record at the same time and there are no noises).
Thank you in advance.
Jp