Hi there
So I'm designing an output filter for the TPA3221 in stereo mode (2x 3ohm load) but having trouble selecting the right inductor. The recommended inductors are:
Coilcraft UA8014-AL
Sagami 7G14J-100M-R / 7G14D-100M-R
However, the availability of the Sagami is poor and the price of the Coilcraft is very high. So I'm looking for alternatives in small form factors.
Would Bournes SRP1265A-100M work ok? The inductance/current curve is fairly flat from 0 to 9A.
Are there any other inductors you can recommend?
Second question:
Originally I was using a 6.8uH + 068uF LC filter as in the TPA3220-MICROEVM. However, this wasn't giving me good results in radiated emissions EMC testing. So I'm going to move to 10uH.
1) What capacitor should I use for 3-ohm load for best EMC results? 1uF? 1.5uF? 2uF? How will this affect idle losses?
2) On the datasheet/evm there are additional filter components: 10nF+3.3r and 1nF. Will these help with EMC?
3) On the datasheet for the TPA3221 is says to use 10nF+3.3r and 1nF but on the schematic for the EVM it says 1uF+3.3r and 1nF. Which is best to use!?
Third question:
Any other tips for improving EMC? I'm already using a 4-layer board, placing the decoupling 1uF caps really close and running the switching outputs on an internal layer.
Thanks