Other Parts Discussed in Thread: TPA3116D2EVM
hi all,
IC: tpa3130d2 PVCC and AVCC = 15V
BD mode, there is no input audio, and the oscilloscope tests any output (single end to ground test) DC = 7.5V, which I think is correct.
1spw mode, no input audio. The oscilloscope tests any output (single end to ground test) and finds that DC = 2.5V. It doesn't feel right. What's the problem?
1psw mode, R51 = ohm, R53 = 5.6k, and the gain is 20dB. I try to input 1kHz sine wave. As expected, the waveform is asymmetrically distorted (single end to ground test).