This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1632: design review please

Part Number: OPA1632
Other Parts Discussed in Thread: OPA1637

Hi there,

I am hoping you could please review and make comment on the preliminary circuit / sketch of our proposed use of the the OPA1632 to provide a unity gain balanced signal line driver.  The input signal is the balanced output from a DAC.  I've asked a separate question in these forums for confirmation on how to power the OPA1632 from a single 12V DC supply, so this will be added to the circuit once I know.

The following is a snippet from our circuit.  Note that I will have 24 differential DAC outputs to feed to 24 x OPA1632's to drive the balanced audio signal to external amplifiers. 

The specification for our audio Codec suggests that at the output of each DAC that a single op amp, 3rd order, low pass filter is recommended.  Is this something we can achieve with the following design using the OPA1632?  Or would I need another op amp ahead of the OPA1632 to achieve this?  We want to maintain the differential / balanced audio signal.  Each output pin of the DAC has a nominal common-mode DC level of 1.5V and swings +/- 1.27 V for a 0 dBFS digital input signal.  Again, will the following design with the OPA1632 accommodate this?

Thank you.

Mark