Hi Expert,
My customer have an issue that is not output from SDOUT with smaller value of BCLK/FSYNC Ratio than 64.
Could you please give me your advice?
Customer want to set MCLK=14.7456MHz, FSYNC_OUT=384kHz and BCLK= 12.288MHz(/or 9.216MHz).
OK setting (but, it is not the configuration customer want)
MCLK=14.7456MHz
BCLK Div Value:3
FSYNC Div Value:64
PLL J-Multi:5
PLL D-Multi:0
Calculated output
BCLK_OUT=24.576MHz
FSYNC_OUT=384.0000kHz
BCLK/FSYNC Ratio=64
NG setting#1
BCLK Div Value:6
FSYNC Div Value:32
Calculated output
BCLK_OUT=12.2880MHz
FSYNC_OUT=384.0000kHz
BCLK/FSYNC Ratio=32
*SDOUT was not output
NG setting#2
BCLK Div Value:8
FSYNC Div Value:24
Calculated output
BCLK_OUT=9.2160MHz
FSYNC_OUT=384.0000kHz
BCLK/FSYNC Ratio=24
*SDOUT was not output
Thanks
Muk